Why can't I find the board FRDM-KE06Z at Debug command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why can't I find the board FRDM-KE06Z at Debug command

2,571件の閲覧回数
修華許
Contributor III
  1. 30102_30102.JPG未命名.JPG
  2. I dont know why it always show NO Device Avaliable?
  3. How should I set to connect to FRDM-KE06Z?
ラベル(1)
10 返答(返信)

2,334件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

After you connect your board , please check here :

pastedImage_0.png

if it is the same with mine , it is right .

Then when debug , check here :

pastedImage_1.png

.

If the two place is different form mine , please show yours , and tell me your PC version , win7 or XP , or else ?

BR

Alice

2,334件の閲覧回数
修華許
Contributor III

I am not very sure the driver, this is my OpenSDA information

jpg4.jpg

0 件の賞賛
返信

2,334件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi ,

From the screenshot of your Device Manger screen , it show the driver have been installed correctly.

While From your screenshot , it have not connected the board :

pastedImage_0.png

So update the bootloader  , do refer to this steps :

pastedImage_1.png

then copy and paste the "MSD-DEBUG-FRDM-KE06Z_Pemicro_v114.SDA" to the bootloader drive .

Then unplug the USB cable and plug it in  again. Then test .

BR

Alice

0 件の賞賛
返信

2,334件の閲覧回数
修華許
Contributor III

Thanks, I've done this before and redo it again.

Still , the same problem occurs.

I choose the debugger console mode,(Among debugger console / No IO / UART)

I guess it's the appropriate options for me, right?

Any other idea for help?

0 件の賞賛
返信

2,334件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The three" console / No IO / UART " are all ok !

It so weird . Please create a simple project and then debug to test .

Or tests the attachment , it is test on my side .

BR

Alice

0 件の賞賛
返信

2,334件の閲覧回数
修華許
Contributor III

Thanks for help .

I am a newbie for freescale MCU. So I am not sure I did the right thing to build your project.

I just drag and .project file to codewarrior .

And press Build All / Then Deubg

still the same problem :smileysad: No idea why?

And one thing to ask ,  I found that the project I build has the word "FLASH" near the project name, is that normal?

I guess my problem is related to Driver, But I have uninstall and reinstall . Still the same

I

0 件の賞賛
返信

2,334件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 修华,

Have your problem been solved ?

"the project I build has the word "FLASH" near the project name, is that normal?" -- yes, it is normal.

And if you still have not solved, i think maybe  your board have some problem , please contact the distribubor,

And you can also  test on other PC , check whether it can work well .

BR

Alice

0 件の賞賛
返信

2,334件の閲覧回数
修華許
Contributor III

Thanks , I solved my problem by install another system.

My original one is WinXP, it didn't work fine.

But I install a WIN7 system , then it works.

But I think the problem is not about OS. Because  found my original DVD disk was gone at XP system.

So I guessed the development board got the same disk name to the original DVD disk

I guessed there are a conflicition between board and DVD disk

Thank you

0 件の賞賛
返信

2,334件の閲覧回数
修華許
Contributor III

jpg3.jpg

0 件の賞賛
返信

2,334件の閲覧回数
修華許
Contributor III

That's mine configuration picturejpg1.JPGjpg2.JPG . I think it's the same

0 件の賞賛
返信