Why can't I drag files into File compare window any more?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why can't I drag files into File compare window any more?

838 Views
phil_b
Contributor I

Using CodeWarrior V5.1, I have always been able to drag files/folders from Windows Explorer into the Compare Files Setup window (Search, File Compare). I recently installed CodeWarrior V10.6.4, so could this have caused the issue?

Labels (1)
0 Kudos
Reply
1 Reply

670 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Phil,

I also have CodeWarrior V10.6.4 and CodeWarrior v5.1 installed on my computer. I can drag file to CW5.1 Compare Files Setup window without problem.

you may try to uninstall CW5.1 then reinstall it, check if this feature can work normally?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply