Hi Pascal,
Thank You very much , Appreciate your kind Help.
The Document you have sujjested provides good information about Caliberating, Debugging of Fressscale MASTER GUI for AUTO A13 and NvmParams
descreption.
It would be great if you can sujjest a document where one can find the RunTimeParms descreptions just like
NvmParams descreption which are available in the document you sujjested.
for example:
the System parameter "Keyfob Avoidance Duration (ms)"
is neatly detailed as below in document
Details:
This parameter defines the length of time the unit will operate at the Keyfob Avoidance Frequency after being
triggered by the IO control signal. This value is ignored if the Keyfob Avoidance Duration Based on IO parameter is
TRUE.
Default Value:
100
Min Value:
0
Max Value:
65535
Member:
NvmParams.SystemParams.OpStateParams.wKeyfobAvoidanceDurationMs
Similarly if one wants to know what does RunTimeparams[0].bySignalStrength or any other RunTimeparams[0].xxxxxxx mean .where can one look for the parameter description?
Thanks & Best Regards,
Santosh