Where did the "target listbox" go ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where did the "target listbox" go ?

ソリューションへジャンプ
1,534件の閲覧回数
udragon
Contributor I
Hi,
 
We recently upgraded from Metrowerks CodeWarrior 3.1 tot Freescale CodeWarrior 6.2 for microcontrollers.
 
I noticed that the 'converted' projects still show the target listbox (which we use allot) but newly create projects only show the 'connection list' .
 
Is there an option somewhere to display the connection list ?
 


Message Edited by udragon on 2008-09-25 09:03 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
561件の閲覧回数
CrasyCat
Specialist III
Hello
 
After reviewing my answer I did realize that I did not answer your question.
In fact you want to add the Connection combo box in a V3.1 project that you have converted to a V6.2 project.
 
This is explained in the same technical note, but in section "Extend a V3.1 project with the new functionality of the V5.0 tool chain ".
 
Sorry for the confusion.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
561件の閲覧回数
CrasyCat
Specialist III
Hello
 
I would look at {Install}\Help\PDF\TN241.pdf (Where {Install} stands for your CodeWarrior installation directory).
There is a section "Using Build Target" -> "4.  Adding Build Target Combo Box to the Project Window " in there explaining how to achieve that.
 
CrasyCat
0 件の賞賛
返信
562件の閲覧回数
CrasyCat
Specialist III
Hello
 
After reviewing my answer I did realize that I did not answer your question.
In fact you want to add the Connection combo box in a V3.1 project that you have converted to a V6.2 project.
 
This is explained in the same technical note, but in section "Extend a V3.1 project with the new functionality of the V5.0 tool chain ".
 
Sorry for the confusion.
 
CrasyCat
0 件の賞賛
返信