Where did the "target listbox" go ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where did the "target listbox" go ?

跳至解决方案
2,005 次查看
udragon
Contributor I
Hi,
 
We recently upgraded from Metrowerks CodeWarrior 3.1 tot Freescale CodeWarrior 6.2 for microcontrollers.
 
I noticed that the 'converted' projects still show the target listbox (which we use allot) but newly create projects only show the 'connection list' .
 
Is there an option somewhere to display the connection list ?
 


Message Edited by udragon on 2008-09-25 09:03 AM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,032 次查看
CrasyCat
Specialist III
Hello
 
After reviewing my answer I did realize that I did not answer your question.
In fact you want to add the Connection combo box in a V3.1 project that you have converted to a V6.2 project.
 
This is explained in the same technical note, but in section "Extend a V3.1 project with the new functionality of the V5.0 tool chain ".
 
Sorry for the confusion.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,032 次查看
CrasyCat
Specialist III
Hello
 
I would look at {Install}\Help\PDF\TN241.pdf (Where {Install} stands for your CodeWarrior installation directory).
There is a section "Using Build Target" -> "4.  Adding Build Target Combo Box to the Project Window " in there explaining how to achieve that.
 
CrasyCat
0 项奖励
回复
1,033 次查看
CrasyCat
Specialist III
Hello
 
After reviewing my answer I did realize that I did not answer your question.
In fact you want to add the Connection combo box in a V3.1 project that you have converted to a V6.2 project.
 
This is explained in the same technical note, but in section "Extend a V3.1 project with the new functionality of the V5.0 tool chain ".
 
Sorry for the confusion.
 
CrasyCat
0 项奖励
回复