When is Freescale going to release a OSBDM dll that will...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When is Freescale going to release a OSBDM dll that will...

ソリューションへジャンプ
2,996件の閲覧回数
UcTechnoGeek
Contributor II
When is Freescale going to release a OSBDM dll that will support the MCF51 Flexis family???

I know the built-in debugger is based on the 9S08 debugger, so the OSBDM hardware should work with the the Flexis coldfire parts.

Are they just trying to protect the margins of the over-priced third party tools or have they given up on the small customers and hobbyist by only offering 1/2 support?

Regards,
Frustrated uCTechnoGeek
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,472件の閲覧回数
osbdm_support
Contributor II
Hello all, I have been recently assigned to support OSBDM on the forums.   We are still having some internal discussion relating to OSBDM, and we are waiting on posting anything to the forums till the discussion is complete.  Please be patient.

Thanks!

Dan Leech
osbdm-support@freescale.com

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,473件の閲覧回数
osbdm_support
Contributor II
Hello all, I have been recently assigned to support OSBDM on the forums.   We are still having some internal discussion relating to OSBDM, and we are waiting on posting anything to the forums till the discussion is complete.  Please be patient.

Thanks!

Dan Leech
osbdm-support@freescale.com
0 件の賞賛
返信
1,472件の閲覧回数
UcTechnoGeek
Contributor II
My appologies to Freescale.

The new CW version 6.2 that was just released does support the OSBDM connection.

Now, we just need to make it work with the OSBDM connection.

uCTechnoGeek
0 件の賞賛
返信
1,472件の閲覧回数
J2MEJediMaster
Specialist I
FWIW, we do have a person recently assigned to handle OSBDM support. I've forwarded this forum thread to him. He's plenty busy, so I can't vouch for when he might get to this. But he has been made aware of the issue.

---Tom

0 件の賞賛
返信