When I try to download the sample project to the Flexis 8...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

When I try to download the sample project to the Flexis 8...

跳至解决方案
2,068 次查看
bobh
Contributor I
When I try to download the sample project to the Flexis 8-bit Demo board I get an script error 45 after the PM command.
 
The cable is connected and the board is running.
 
Does anyone know how to correct this error and download the frimware to the board ?
 
 
                                            Thanks,
                                            Bob H
标签 (1)
标记 (1)
0 项奖励
1 解答
543 次查看
CrasyCat
Specialist III
Hello
 
There seem to be a similar post on P&E forum.
 
Look at
 
 
CrasyCat

在原帖中查看解决方案

0 项奖励
3 回复数
543 次查看
J2MEJediMaster
Specialist I
Sorry, I can't help you with this. However, you can help others help you by mentioning the MCU part number and version of CodeWarrior that you're using in the subject line. Forum users don't know what you're working with and may just skip over your post due to the lack onf information.

---Tom
0 项奖励
543 次查看
bobh
Contributor I
1. cw ver 5.9.0 build 2330.
2. pemicro demoqe rev a
3.  mc9s08qe128
 
I am getting an script error 45 when I try to download an example project though my UBS port.
Does anyone know the reason.
 
                                    Thanks,
                                    Bob H
 
  
0 项奖励
544 次查看
CrasyCat
Specialist III
Hello
 
There seem to be a similar post on P&E forum.
 
Look at
 
 
CrasyCat
0 项奖励