When I try to download the sample project to the Flexis 8...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When I try to download the sample project to the Flexis 8...

ソリューションへジャンプ
2,298件の閲覧回数
bobh
Contributor I
When I try to download the sample project to the Flexis 8-bit Demo board I get an script error 45 after the PM command.
 
The cable is connected and the board is running.
 
Does anyone know how to correct this error and download the frimware to the board ?
 
 
                                            Thanks,
                                            Bob H
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
773件の閲覧回数
CrasyCat
Specialist III
Hello
 
There seem to be a similar post on P&E forum.
 
Look at
 
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
773件の閲覧回数
J2MEJediMaster
Specialist I
Sorry, I can't help you with this. However, you can help others help you by mentioning the MCU part number and version of CodeWarrior that you're using in the subject line. Forum users don't know what you're working with and may just skip over your post due to the lack onf information.

---Tom
0 件の賞賛
返信
773件の閲覧回数
bobh
Contributor I
1. cw ver 5.9.0 build 2330.
2. pemicro demoqe rev a
3.  mc9s08qe128
 
I am getting an script error 45 when I try to download an example project though my UBS port.
Does anyone know the reason.
 
                                    Thanks,
                                    Bob H
 
  
0 件の賞賛
返信
774件の閲覧回数
CrasyCat
Specialist III
Hello
 
There seem to be a similar post on P&E forum.
 
Look at
 
 
CrasyCat
0 件の賞賛
返信