What was changed from CW 6.0 to 6.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What was changed from CW 6.0 to 6.1?

Jump to solution
3,621 Views
UcTechnoGeek
Contributor II
What was changed from CW 6.0 to 6.1?
When is Freescale going to add OSBDM support for the ColdFire V1 devices?

uCTechnoGeek
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,272 Views
CrasyCat
Specialist III
Hello
 
Changes between V6.0 and V6.1 are documented in file "Welcome_CW_MCUs.txt", which is located in your V6.1 installation directory.
 
I will try to find out what are the plans around support for OSBDM.
 
CraysCat
 

View solution in original post

0 Kudos
Reply
3 Replies
1,273 Views
CrasyCat
Specialist III
Hello
 
Changes between V6.0 and V6.1 are documented in file "Welcome_CW_MCUs.txt", which is located in your V6.1 installation directory.
 
I will try to find out what are the plans around support for OSBDM.
 
CraysCat
 
0 Kudos
Reply
1,272 Views
UcTechnoGeek
Contributor II
Thanks. :smileyhappy:

I was just trying to avoid downloading the "mega file", just to find out what changed.

Would Freescale consider adding a "here's what changed" to the website, so we can see if we want to upgrade before downloading the program?

It has gotten much better, but in the past you could spend days "fixing" your project, just because you upgraded the IDE.

uCTechnoGeek
0 Kudos
Reply
1,272 Views
CrasyCat
Specialist III
Hello
 
Will suggest that to our marketing people.
 
In the mean time, find attached the text file describing changes between V6.0 & V6.1
 
CrasyCat
0 Kudos
Reply