What was changed from CW 6.0 to 6.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What was changed from CW 6.0 to 6.1?

ソリューションへジャンプ
3,669件の閲覧回数
UcTechnoGeek
Contributor II
What was changed from CW 6.0 to 6.1?
When is Freescale going to add OSBDM support for the ColdFire V1 devices?

uCTechnoGeek
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,320件の閲覧回数
CrasyCat
Specialist III
Hello
 
Changes between V6.0 and V6.1 are documented in file "Welcome_CW_MCUs.txt", which is located in your V6.1 installation directory.
 
I will try to find out what are the plans around support for OSBDM.
 
CraysCat
 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,321件の閲覧回数
CrasyCat
Specialist III
Hello
 
Changes between V6.0 and V6.1 are documented in file "Welcome_CW_MCUs.txt", which is located in your V6.1 installation directory.
 
I will try to find out what are the plans around support for OSBDM.
 
CraysCat
 
0 件の賞賛
返信
1,320件の閲覧回数
UcTechnoGeek
Contributor II
Thanks. :smileyhappy:

I was just trying to avoid downloading the "mega file", just to find out what changed.

Would Freescale consider adding a "here's what changed" to the website, so we can see if we want to upgrade before downloading the program?

It has gotten much better, but in the past you could spend days "fixing" your project, just because you upgraded the IDE.

uCTechnoGeek
0 件の賞賛
返信
1,320件の閲覧回数
CrasyCat
Specialist III
Hello
 
Will suggest that to our marketing people.
 
In the mean time, find attached the text file describing changes between V6.0 & V6.1
 
CrasyCat
0 件の賞賛
返信