What to do once no interrupt to handle for XGATE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What to do once no interrupt to handle for XGATE?

1,976 Views
HUST
Contributor I
Hi ,I wonder what to do while no interrupt to deal with for xgate module? Idle or sleep or active for NOP? thanks 
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,034 Views
HUST
Contributor I
9s12XE,   will  the xgate  keep running   afer enable, which means consume the power?  or, the xgate will automatically enter the sleep(standby) mode after the interrupt finished to save the power?
0 Kudos
Reply

1,034 Views
admin
Specialist II
Greetings, are not clear a question not much.... In general Xgate it is developed for fast interrupt processing. You use what processor? Esteem in datashete there all should be written...
0 Kudos
Reply