Warning C1801: Implicit parameter-declaration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Warning C1801: Implicit parameter-declaration

跳至解决方案
11,060 次查看
BasePointer
Contributor II
Hi,
 
I'm using CW6.0 and HCS08 C.
The compiler generates warnings for my application "Warning C1801: Implicit parameter-declaration".
And this warning causes my application not to work properly.
 
I want to take compile error with this warning. Is this possible?
 
Thanks.
 
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
4,733 次查看
BlackNight
NXP Employee
NXP Employee
Hi,
yes, there is a #pragma way for this

something like
#pragma MESSAGE ERROR C1801
(see manual/help files for details).

The other way is to use the
#pragma OPTION ADD xx "-Wpd"
way.

BK

在原帖中查看解决方案

0 项奖励
回复
7 回复数
4,733 次查看
BasePointer
Contributor II
Hi,
 
Standard Settings... -> Compile for HC08 -> Messages -> Warning Tab and I moved C1801 to the Error.
 
Now I'm taking compile error with C1801. This is exactly what I want.
 
Thank you.
BP.
0 项奖励
回复
4,733 次查看
BlackNight
NXP Employee
NXP Employee
Hello,
there is as well the compiler option
-Wpd          Error for implicit parameter declaration
under the MESSAGE tab which will flag implicit parameter declarations as error.

BK
0 项奖励
回复
4,733 次查看
BasePointer
Contributor II
Hi,
 
 I also wonder if I can do this with #pragma directions?
 
Thanks.
0 项奖励
回复
4,734 次查看
BlackNight
NXP Employee
NXP Employee
Hi,
yes, there is a #pragma way for this

something like
#pragma MESSAGE ERROR C1801
(see manual/help files for details).

The other way is to use the
#pragma OPTION ADD xx "-Wpd"
way.

BK
0 项奖励
回复
4,733 次查看
BasePointer
Contributor II
That works:
#pragma MESSAGE ERROR C1801     // Implicit parameter declaration
 
Thank you so much.
0 项奖励
回复
4,733 次查看
Alban
Senior Contributor II
Hello,

It is possibke to compile without warnings.
The fault is not because of the warning, but probably because you use a function in your code and you did not declare the function prototype before.

Warning and Error codes are very useful as they are described in the help of CodeWarrior.

C1801 means Compiler error. Lxxxx would mean a linker error...

Alban.
0 项奖励
回复
4,733 次查看
BasePointer
Contributor II
Hi Alban,
 
My project is huge and as you said I sometimes forget adding functions prototypes.
I can compile entire project successfully even if I did so.
I want compile process to fail if this warning exists for any modules of the project.
 
Or can I see all warings of modules in a list?
I can easly search C1801 in this list.
 
Regards,
BP.
0 项奖励
回复