I have never used this facility before, so a LOT of help would be useful. I am using a S08QE with a MUltilink FX (I also have a DEMOQE128 if necessary).
I am developing a control application and I need to download data acquisition (probably ~4K) from the target for analysis on my computer.
How can I use the Virtual Comm utility do do this? Do I need code in my application in order to communicate serially, or does the BDM interface take care of it? The P&E documentation is a bit light on detail.
I have a 64-bit Windows 7 and so the P&E utilities will not install.
解決済! 解決策の投稿を見る。
I don't know why, but I downloaded it three times an on the third time I got the same version as you and now it works fine. Thanks.
I don't know why, but I downloaded it three times an on the third time I got the same version as you and now it works fine. Thanks.
OK!
BR
Alice
Thank you for your help. However, I cannot install the Virtual Serial Toolkit as it is not compatible with 64- bit Windows, (or is there a 64-bit version?)
Hello Julian,
My PC is Win10 64 bit, I can install it without any problem.
I download from PEmicro site : http://www.pemicro.com/osbdm/ , please have a look at attachment.
What about the problem when you install ? Please take a screenshot about the errro .
You can also search the error reminder in PEmicro support site :http://www.pemicro.com/support/index.cfm
BR
Alice
As requested, Attached is the screenshot.it stays like this - no progress - until I select OK
It then rolls back the installation
Hello Julian,
It seems your tool version is not the same with mine:
I download from : http://www.pemicro.com/osbdm/
BR
Alice
Hello Julian,
- The "Virtual serial " is intergrated in OSBDM/OSJTAG debug of NXP( Freescale) tower board,
that is to say if you use the demo board of freescale, there is a Virtual serial in tower board, so the microcontroller can output data to PC.
While the external debugger MUltilink FX only has debug function, if you want to send data ,
you can use the Serial Communications Interface .
About the detail , please have a look at "OSBDM_OSJTAG_Virtual_Serial_Toolkit_Resources.pdf" .
- If you use CodeWarrior IDE, you can create a proejct based Processor Expert ,then add the "AsynchroSerial" component ,there is demo code 。
Hope it helps
Alice