Using crystal on DEMO board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using crystal on DEMO board

跳至解决方案
1,315 次查看
Iain
Contributor I

CW 5.9, HCS08QE32, DEMOQE

 

I wish to have a 1000Hz clock for TPM timing, and it was suggested by a forum member that that I should set my TPM to use 32kHz crystal XCLK, and prescaler of 32 to give me my 1000Hz clock, and that, I understand. 

Below is code I have to set the ICS (HCS08QE has no ICG).

 

 

ICSC1 = 0b10000000;  // CLKS = 10 external referenceICSC2 = 0b00000110;  // EREFS = 1 oscillator driving crystal,                     // ERCLKEN = 1 ICSERCLK enabledwhile(!ICSSC_OSCINIT){} // wait for external crystal to be initiallised

 

 

I am getting confused by internal/external references, there seems to be more options than I thought there would be, also the EREFS bit I am unsure of, as the book I am using and data sheet seem to contradict each other when mentioning oscillators/crystals/resonators.

 

Basically I just want to set the micro to make use of the 32kHz crystal on my demo board (attatched to EXTAL and XTAL pins),  but am not sure if I am setting the registers correctly, can anyone help?

 

Regards,

Iain

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
782 次查看
bigmac
Specialist III

Hello Iain,

 

I had a closer look at the ICS section in the reference manual, and the fixed frequency clock source is derived differently compared with some of the other HCS08 devices.  For the QE device, the fixed frequency clock, as an alternate clock source for the TPM modules, is derived from the current reference source, whether internal or divided external source.  For other devices, the external source is used.  This means that it would seem possible to use either FEI mode or FEE mode to generate the bus frequency, and also provide the alternate TPM clock.

 

I also see that there is an additional frequency division by 2, before the clock is applied to the TPM prescaler, that I had previously overlooked. This means that the clock frequency will be nominally 16 kHz.

 

Accepting that you still require to use an external reference, I believe that the ICSC1 value should be 0x00 in order to source the bus clock from the FLL.  A setting of 0x80 would be causing FBE mode, giving a 16 kHz bus frequency  - not what you require.   A nominal bus frequency of 4 MHz should be achieved with ICSC2 = 0x44; and ICSSC = 0x00;

i.e. Bus frequency = 32768 * 512 / 2 / 2

 

Regards,

Mac

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
783 次查看
bigmac
Specialist III

Hello Iain,

 

I had a closer look at the ICS section in the reference manual, and the fixed frequency clock source is derived differently compared with some of the other HCS08 devices.  For the QE device, the fixed frequency clock, as an alternate clock source for the TPM modules, is derived from the current reference source, whether internal or divided external source.  For other devices, the external source is used.  This means that it would seem possible to use either FEI mode or FEE mode to generate the bus frequency, and also provide the alternate TPM clock.

 

I also see that there is an additional frequency division by 2, before the clock is applied to the TPM prescaler, that I had previously overlooked. This means that the clock frequency will be nominally 16 kHz.

 

Accepting that you still require to use an external reference, I believe that the ICSC1 value should be 0x00 in order to source the bus clock from the FLL.  A setting of 0x80 would be causing FBE mode, giving a 16 kHz bus frequency  - not what you require.   A nominal bus frequency of 4 MHz should be achieved with ICSC2 = 0x44; and ICSSC = 0x00;

i.e. Bus frequency = 32768 * 512 / 2 / 2

 

Regards,

Mac

 

0 项奖励
回复