Using MK66FN2M0VLQ18 in place of MK64FN1M0VMD12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MK66FN2M0VLQ18 in place of MK64FN1M0VMD12

776 Views
anoojas
Contributor I

The project i am working now uses  MK64FN1M0VMD12  as  device. Now i want to replace it with  MK66FN2M0VLQ18. I am using codewarrior 10.6. I just want to know how it can be done.

Labels (1)
0 Kudos
Reply
1 Reply

589 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

I think the best way is creating a new project about  MK66FN2M0VLQ18,

then copy and paste the application code into it , build and fix error, debug to

check whether function can work well .


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply