Project is going very well. Basically I helped created a Kinetis L design that will control a lighting solution. Questions for the Kinetis KL05 series that are still outstanding:
1. Can we make our own K20 open SDA programmer/debugger just like what is used on the FRDM board? I saw some other discussions and it seems that the FRDM board is locked, i.e. the K20 expects one unique KL device only. This would allow customers to make their own factory programmers.
2. Bootloaders - customers would pay extra for a Kinetis L part that would support usb boot loader. This way you have a micro usb connector on their product and it would support field upgrades. Having only i2c bootloader available is sort of sad in that they now have to build a usb or serial to i2c converter.
3. For 8 bit customers migrating to Kinetis L, the clock tree is very confusing. It would be nice to have as a simple program like Excel which asked what core clock you want and what bus speed you want and it shows you the different configurations that would get you there with the FEI, FEE, FBI, FBE, BLPI, BLPE clock tree.