Hello,
I'm looking for a good alternative to debug the PowerPC microcontroller SPC5668E. One alternative would be to use CW 10.6 together with P&E Micro's debug probe (U-MULTILINK or U-MULTILINK-FX).
Does anyone have experience with this setup?
I would also like to know if an 14-Pin Berg to 38-Pin Mictor Adaptor (like http://www.pemicro.com/products/product_viewDetails.cfm?product_id=159 ) is included if I buy U-MULTILINK or U-MULTILINK-FX? I have a 38-pin mictor on the PCB.
What debug features are included in CW 10.6?
Can I set a breakpoint while the programming is running?
Can I get live update on variables?
Callstack?
Can I change variables etc.?
Write to HW registers?
Is trace included?
Can I program the device with CW 10.6?
Kind regards,
Jonas
Hello Jonas
It is a same question with this one:
Best Regards
Fiona Kuang
Technical Information & Commercial Support