Upload CW 10.6.4 project to FRDM-KE06Z using Windows 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Upload CW 10.6.4 project to FRDM-KE06Z using Windows 10

ソリューションへジャンプ
1,386件の閲覧回数
manuelrabia
Contributor II

I have a little project on CodeWarrior 10.6.4 for FRDM-KE06Z board and I've been trying to upload it to the board unsuccessfully. I'm not sure if it's possible to do it pluggin the board directly to the usb pc port with a previous driver installed, or if it's necessary an additional hardware. 

 

I'll be thankful to know the method to do this, it's the last step to make this project work.

 

Best Regards.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,205件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Manuel,

have you loaded the OpenSDA debug firmware on your board already (P&E or Segger)?

See Illustrated Step-by-Step Instructions: Updating the Freescale Freedom Board Firmware | MCU on Eclips...

If not, you cannot debug the board as from the factory it comes with no debug firmware loaded.

But there will be a problem for you: you need a Windows 7 machine to update the bootloader (the bootloader does not work without update on Windows 10), see above post.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,206件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Manuel,

have you loaded the OpenSDA debug firmware on your board already (P&E or Segger)?

See Illustrated Step-by-Step Instructions: Updating the Freescale Freedom Board Firmware | MCU on Eclips...

If not, you cannot debug the board as from the factory it comes with no debug firmware loaded.

But there will be a problem for you: you need a Windows 7 machine to update the bootloader (the bootloader does not work without update on Windows 10), see above post.

I hope this helps,

Erich

0 件の賞賛
返信
1,205件の閲覧回数
manuelrabia
Contributor II

Thank you very much Erich.

I have a last little doubt, once I have updated the bootloader and firmware on Windows 7, will I be able to degug on Windows 10 too or the communication between CW 10.6.4 and the board works only on Windows 7.

0 件の賞賛
返信