UART TX interrupt not occured

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART TX interrupt not occured

Jump to solution
2,029 Views
olegivanus
Contributor III

Hello everyone,

Why does UART not cause interrupt handler?

Look at my project below

Thank you!

Original Attachment has been moved to: UART.zip

Labels (1)
0 Kudos
Reply
1 Solution
1,735 Views
Rick_Li
NXP Employee
NXP Employee

Hi Oleg,

the silicon you are using is MPC5643, I have forward this issue to my another colleague and she will help you on it!

Regards,

Yong

View solution in original post

0 Kudos
Reply
4 Replies
1,735 Views
Rick_Li
NXP Employee
NXP Employee

Hello Oleg,

I'm sorry, could you please re-upload your UART.zip?

The project you attached can't be downloaded!

0 Kudos
Reply
1,733 Views
olegivanus
Contributor III

Hello, Yong Li

See attachment below)

Thanks

0 Kudos
Reply
1,736 Views
Rick_Li
NXP Employee
NXP Employee

Hi Oleg,

the silicon you are using is MPC5643, I have forward this issue to my another colleague and she will help you on it!

Regards,

Yong

0 Kudos
Reply
1,733 Views
olegivanus
Contributor III

Thank you!

0 Kudos
Reply