Hi,
I have recently installed CW professional Version 8.8.
After the installation, I used the CW updater to install the service pack " CodeWarrior
Power Architecture 8.8 Service Pack 2” for MPC8306, MPC8308 and MPC8309." (since I intend to used CW on the MPC8309kit board).
When I start the flash programmer (tools/flash programmer/Target Configuration), the target processor 8309 is not available in the 83xx family.
Question:
What should I do more in order to add the target processor 8309 to the 83xx family?
Thanks
  
Thank you for your reply Pavel.
But as I am saying in the description, I have done what you suggested but it is still not helping.
So I guess there is something else I ned to do.
Load and install the CW PA v8.8 for 830606S-8308-8309 Windows-hosted Service Pack.
See attached snapshot.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------