Tab Expansion in Hiwave Debugger (HCS12(X) V4.7)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tab Expansion in Hiwave Debugger (HCS12(X) V4.7)

ソリューションへジャンプ
1,705件の閲覧回数
djsimpson
Contributor III

Is there any way to change the default tab expansion in the Hiwave debugger from the default of four? I would like to set it to eight, which matches the source files I am working with.

 

I am running the debugger standalone, and not from the IDE.

 

Thanks

 

David

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,091件の閲覧回数
CrasyCat
Specialist III

Hello

 

As far as I know this is not possible with the debugger today.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,092件の閲覧回数
CrasyCat
Specialist III

Hello

 

As far as I know this is not possible with the debugger today.

 

CrasyCat

0 件の賞賛
返信