Tab Expansion in Hiwave Debugger (HCS12(X) V4.7)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tab Expansion in Hiwave Debugger (HCS12(X) V4.7)

Jump to solution
1,071 Views
djsimpson
Contributor III

Is there any way to change the default tab expansion in the Hiwave debugger from the default of four? I would like to set it to eight, which matches the source files I am working with.

 

I am running the debugger standalone, and not from the IDE.

 

Thanks

 

David

Labels (1)
Tags (1)
0 Kudos
1 Solution
457 Views
CrasyCat
Specialist III

Hello

 

As far as I know this is not possible with the debugger today.

 

CrasyCat

View solution in original post

0 Kudos
1 Reply
458 Views
CrasyCat
Specialist III

Hello

 

As far as I know this is not possible with the debugger today.

 

CrasyCat

0 Kudos