TBDML and CW5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TBDML and CW5.1

Jump to solution
2,256 Views
bricofab
Contributor I
Hello,

I've made a TBDML and I've installed it on my computer but when I use it with a S08QG4, there is no work. I write "set gdi" on the command windows, I configure the good dll but it never work.
Does someone have an experience with TBDML and CW5.1?

Thanks a lot for your help.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,138 Views
eckhard
Contributor V
Hello,

TBDML is only for the hcs12 controller family. If you want to programm a mc9s08 controller ou should check OSBDM.

Eckhard

View solution in original post

0 Kudos
Reply
2 Replies
1,139 Views
eckhard
Contributor V
Hello,

TBDML is only for the hcs12 controller family. If you want to programm a mc9s08 controller ou should check OSBDM.

Eckhard
0 Kudos
Reply
1,138 Views
bricofab
Contributor I
And is OSBDM running with CW5.1? It is noticed that it's running with 5.0 but no informations with 5.1.
 
Thanks for your help.
 
Bricofab
0 Kudos
Reply