Sudden Error Shown: "An internal error occurred during: "Debug Database Initialization"."

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sudden Error Shown: "An internal error occurred during: "Debug Database Initialization"."

ソリューションへジャンプ
1,873件の閲覧回数
dcongie
Contributor I

I've been using CodeWarrior 10 for several years however recently I received an error which prevents me to perform Flash Program or debugging.

The error is showing at the start of the IDE even there's no project opened.

cw error.png

I've tried uninstalling and installing the Microsoft Visual C++ Redistriutable packages but it seems not related to the problem.

I've attached the diagnostics for more information.

0 件の賞賛
返信
1 解決策
1,753件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Donald,

Please check if solution in this link can also work you.

https://community.nxp.com/message/368501 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,754件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Donald,

Please check if solution in this link can also work you.

https://community.nxp.com/message/368501 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,753件の閲覧回数
dcongie
Contributor I

I followed the instruction to delete the .metadata folder and it fixed my issue.

Thanks!

0 件の賞賛
返信
1,753件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi dcongie,

Good! Thanks for the sharing.

Best Regards

Jun Zhang

0 件の賞賛
返信