Sudden Error Shown: "An internal error occurred during: "Debug Database Initialization"."

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sudden Error Shown: "An internal error occurred during: "Debug Database Initialization"."

Jump to solution
1,813 Views
dcongie
Contributor I

I've been using CodeWarrior 10 for several years however recently I received an error which prevents me to perform Flash Program or debugging.

The error is showing at the start of the IDE even there's no project opened.

cw error.png

I've tried uninstalling and installing the Microsoft Visual C++ Redistriutable packages but it seems not related to the problem.

I've attached the diagnostics for more information.

0 Kudos
Reply
1 Solution
1,693 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Donald,

Please check if solution in this link can also work you.

https://community.nxp.com/message/368501 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
1,694 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Donald,

Please check if solution in this link can also work you.

https://community.nxp.com/message/368501 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,693 Views
dcongie
Contributor I

I followed the instruction to delete the .metadata folder and it fixed my issue.

Thanks!

0 Kudos
Reply
1,693 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi dcongie,

Good! Thanks for the sharing.

Best Regards

Jun Zhang

0 Kudos
Reply