Some more little problems with PE's simulator in CW 5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Some more little problems with PE's simulator in CW 5.1

3,849 次查看
joerg
Contributor II
Hi
since i am a "simulator" i noticed some more problems with the PE simulator:

For HC08QBx: the ADDI and the ADCLR commands are not implemented -> Error: No such command.

For HCS08QD4: simulator does not know this device in the patched CW 5.1 version (device is
missing!) (it is hard to figure out the real version of the CW i think it is
the version 5.7....). the strange thing is that it worked before i have
updated it recently.

I hope the version 5.2 will work!

Saluti Joerg
标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

1,691 次查看
Phoenix
Contributor III
Hi Joerg,
 
1) ADDI and ADCLR ? I did not found this instruction in QBx datasheet
 
2) I have CW 5.1. with last patches and QD4 is present in simulator.. Strange.
Could you log ServiceRequest for this? Attach full version description to it.
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products
Provide us all info displayed.
Or you can save them in a txt file.
 
Thanx
0 项奖励
回复

1,691 次查看
joerg
Contributor II
Hi Phoenix

ADDI and ADCLR are simulation commands to load the AD values into a simulation. They are not MPU commands. PE has simply forgotten to implemet them. I have also written a service request for that case.

The QD4 simulation is working now. I had to download the QD4 update again. I think the recent update function did not download this patch -> Thanks Nina!

Saluti Joerg
0 项奖励
回复

1,691 次查看
Phoenix
Contributor III
Thankx for info. Do you log the SR directly to PE or to Freescale (in this case what is SR number please?)
0 项奖励
回复

1,691 次查看
joerg
Contributor II
Hi
the QD4 stuff has the SR 1-338055551 ID and
the QBx SR is 1-338048561

Thanks Joerg
0 项奖励
回复

1,691 次查看
joerg
Contributor II
Hi
today i noticed that in the QD4 patch the OSBDM08 is not included!
Could you fix this!

Saluti Joerg
0 项奖励
回复

1,691 次查看
CrasyCat
Specialist III
Hello
 
I would highly recommend you to submit the defect to either P&E or to Freescale if you want to make sure the issue is fixed in next build.
 
To log the issue with P&E, go to their Web site (www.pemicro.com) and use their support page to log the issue.
 
You need to submit a service request  for that.
 
To log the issue with Freescale please go to following URL:
    http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=054670&tid=FSH
and click on "Submit a service request"
 
CrasyCat
0 项奖励
回复

1,691 次查看
joerg
Contributor II
Dear CrasyCat
i know that, but i think ti is important for other users to kown such issues.
It would be nice if the forwarding of this kind of errors goes directly this way.

Saluti Joerg
0 项奖励
回复