Setting up CW 11 for specific dev board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting up CW 11 for specific dev board?

1,930 次查看
zwilcox
Contributor IV

I'm using a M54451EVB development board.  I'm asked for the derivative or board I would like to use:
new project.JPG

However, it is unable to find my board.  In fact, when I expand all the options, it doesn't look like there are any boards in there.

Is there a way to set up a project to use the a specific dev board, particularly the M54451EVB?

Thank you.

0 项奖励
回复
7 回复数

1,697 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

You create a "New bare board project"  which doesn't support selecting board as target, thus you can select chip dirivative only. The "board" you highlighted confuses users. I will report it.

If user use SDK or MQX, board can be selected. but we need check if the SDK or MQX supports this board.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,697 次查看
zwilcox
Contributor IV

Thank you for your reply. 

MQX is an RTOS right?  I need to have a bare metal project.


Which SDK are you referring to?

0 项奖励
回复

1,697 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zachary

yes, MQX is RTOS.

See SDK here

MCUXpresso SDK|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,697 次查看
zwilcox
Contributor IV

Thank you for your help.  But I'm unable to use an RTOS and MCUXpresso does not support my board. 

0 项奖励
回复

1,697 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, MCUXpresso doesn't support codefire.

you use Coldfire M54451EVB , you need use CodWarrior. I just checked MQX doesn't support his board.

As I know we do not have any plan for MQX to support M54451EVB.(Only the M54455EVB are supported in MQX4.x.)


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,697 次查看
zwilcox
Contributor IV

Right.  I am using ColdWarrior.  And have no plans to use MXQ.

0 项奖励
回复

1,697 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

If don't use MQX, we can only choose "derivative" only.

0 项奖励
回复