Setting Security for MC9S98GB60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting Security for MC9S98GB60

4,405 Views
fef
Contributor I
I am using CW IDE 5.7.0 with a PnE Multilink USB adapter, and I need to set the security bits to lock the flash. I would like to do this when the code is loaded into the processor. However, I can't figure out how to have the programmer set the security bits. Any suggestions are appreciated.
Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

1,249 Views
fef
Contributor I
It does seem a bit unusual that CW does not support FLASH security control, but thanks to the suggestions from Rocky, I seem to have accomplished the desired goal. However, I believe the value $40 should be used for NVOPT to disable vector redirection. Thanks for the help.

fef
0 Kudos
Reply

1,249 Views
peg
Senior Contributor IV

Hi,

Well, it appears RockyRoad has hit a bit of a rough patch (get it?). Still 1 out 4 is better than none!

 


KEYEN — Backdoor Key Mechanism Enable

When this bit is 0, the backdoor key mechanism cannot be used to disengage security. The backdoor

key mechanism is accessible only from user (secured) firmware. BDM commands cannot be used to

write key comparison values that would unlock the backdoor key. For more detailed information about

the backdoor key mechanism, refer to Section 4.5, “Security.”

1 = If user firmware writes an 8-byte value that matches the nonvolatile backdoor key

(NVBACKKEY through NVBACKKEY+7, in that order), security is temporarily disengaged

until the next MCU reset.

0 = No backdoor key access allowed.

FNORED — Vector Redirection Disable

When this bit is 1, vector redirection is disabled.

1 = Vector redirection disabled.

0 = Vector redirection enabled.

SEC01:smileyfrustrated:EC00 — Security State Code

This 2-bit field determines the security state of the MCU as shown in Table 4-7. When the MCU is

secure, the contents of RAM and FLASH memory cannot be accessed by instructions from any

unsecured source including the background debug interface. For more detailed information about

security, refer to Section 4.5, “Security.”

0:0   secure

0:1   secure

1:0   unsecure

1:1   secure

SEC01:smileyfrustrated:EC00 changes to 1:0 after successful backdoor key entry or a successful blank check of FLASH.



Regards David

 

Message Edited by peg on 06-04-2006 09:22 AM

0 Kudos
Reply

1,249 Views
RockyRoad
Contributor III

I have to correct my answer. A colleague of mine challenged my answer to this. Here's what I've learned since my previous post.

CodeWarrior and the Multilink program NVPROT to $FE (unsecured). This is how you can still see flash and debug after programming. (This should have been obvious, but I've missed it all this time.)

Some new important information that I've also learned is that since SEC01:smileyfrustrated:EC00 is already programmed to 1:0, then the only secure combination that you can use is 0:0. This is because this programming takes place without erasing and you can only change the 1 to a 0. (You get an Error 18 during the programming if for example you try 1:1.)

So a better example of the code fragment to include in your source code that shows actually setting security would be:

;Configure Security
          ORG  NVOPT                ; $FFBF
          DC.B      $00             ; secure, no backdoor key, no vector redirection

My apologies for my incorrect original posting.

- Rocky

 

0 Kudos
Reply

1,249 Views
peg
Senior Contributor IV

Hi,

The inability to secure a device is purely a Codewarrior limitation!

It is fully supported by the Multilink and the P&E software.

If you use expert programmer mode you can do it from there.

It could be done automatically through the commandline programmer too if the facility to generate the required command in the script was provided within hiwave/codewarrior.

Regards David

 

0 Kudos
Reply

1,249 Views
RockyRoad
Contributor III

Welcome to the forum!

The erased state of the SEC01:smileyfrustrated:EC00 bits is secured (1:1). The only unsecure combination is 1:0. So you can just leave them alone and the flash will be secured after a reset.

CodeWarrior and the Multilink don't provide an automatic method to set security (or any of the other flash-based registers). You need to do this in your code. In assembly, I do it like this (unsecuring it in this case):

;Configure Security
          ORG  NVOPT                ; $FFBF
          DC.B      $02             ; not secure

- Rocky

0 Kudos
Reply