Setting Output Compare with MC9S12C32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting Output Compare with MC9S12C32

ソリューションへジャンプ
1,853件の閲覧回数
maurix1966
Contributor I
Hello!
 
I'm new with Freescale.
I've a problem with a MC9C12C32.
The question is:
how i can set , with processor expert, a pin to be an output compare?
 
I've tried with Processor Expert and i can only set a pin to be an Input Capture but not Output Compare.
 
Thank you for help.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,046件の閲覧回数
CrasyCat
Specialist III
Hello
 
I have created a project for HCS12C32 and if I add a "TimeOut" Bean, I am able to define PT0_PWM0_IOC0 as output pin.
 
I am using CodeWarrior for HC12 V4.5
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,047件の閲覧回数
CrasyCat
Specialist III
Hello
 
I have created a project for HCS12C32 and if I add a "TimeOut" Bean, I am able to define PT0_PWM0_IOC0 as output pin.
 
I am using CodeWarrior for HC12 V4.5
 
CrasyCat
0 件の賞賛
返信