SERIOUS problem with CW 5.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SERIOUS problem with CW 5.0

Jump to solution
2,380 Views
peblink
Contributor I
Hello, I used to work with CW v3.1 but i decided to upgrade to CW 5.0 (eval)but i had a serious problem when i installed CW 5.0 because it deleted some important system files in my PC and i couldnt start it anymore so I had to restore everything and it was really awful.

Anyway, I wanted to work again with CW v3.1, but now my code is a bit larger than the one allowed by the original license (1k, my actual code size is 1043 bytes)I kept a license that allowed larger size but now it doesnt work anymore (When I start CW it tells me i need a license)

Can you please help me? As you can see I dont want to use v5.0, I cant risk another computer blow. I attached the license i got about 2 yrs ago for larger size

Thanks a lot



#
# This license file contains a limited IDE license Win32_CWIDE_Limited below).
# With this limited (demo) license, the IDE is limited (maximum of 32 files
# in a project, no creation of subtargets.
# With the registered product, you will get a license for an unlimited IDE.
#
# Without having additional license keys, the software will run in a
# limited demo mode only (code size restricted).
# To get a free 30 day evaluation license, please run the
# 'Register CodeWarrior' shortcut created by the installation
# in the corresponding CPU target subolder in your start menu.
# If you get license entries, they can be added below using a text editor.
#

FEATURE Win32_CWIDE_Limited metrowks 4.2 permanent uncounted \
2C3C43468173 HOSTID=ANY

FEATURE Win32_CWIDE_Limited metrowks 4.2 permanent uncounted 2C3C43468173 HOSTID=ANY
#######################################################
# CWHC08SE: CodeWarrior HC08 Special Edition
# IDE: learning edition (max 32 files, no subprojects).
# Build/Debug: Unlimited Assembly/Hex/S19. C code up to 4K. ELF/Dwarf object file format.
# Target Interface: PEDebug, MMDS/MMEVS.
# Processor Expert: basic beans.
#######################################################
FEATURE ProcessorExpertHC08 metrowks 1.000 permanent uncounted 32B6630AF9FC VENDOR_STRING="Basic beans;3BB9A2004454C1C59475110BC0E35B7C" HOSTID=ANY ck=149
FEATURE HI001300 metrowks 2.000 permanent uncounted 96FDA86A96FE VENDOR_STRING=Burner HOSTID=ANY ck=166
FEATURE HI005250 metrowks 2.000 permanent uncounted 7A2516346543 VENDOR_STRING="HC08 MMDS Target" HOSTID=ANY ck=94
FEATURE HI044011 metrowks 2.000 permanent uncounted F890E15B6BFC VENDOR_STRING="Hexadecimal Loader" HOSTID=ANY ck=139
FEATURE HI100100 metrowks 2.000 permanent uncounted BD004FFE088D VENDOR_STRING="4096 bytes of code, HC08 Compiler ANSI-C" HOSTID=ANY ck=166
FEATURE HI100140 metrowks 2.000 permanent uncounted 277242C7A62F VENDOR_STRING="HC08 Macro Assembler" HOSTID=ANY ck=106
FEATURE HI100150 metrowks 2.000 permanent uncounted F446372DDE6D VENDOR_STRING="4096 bytes of C code, 1024 bytes of C++ code, HC08 Linker" HOSTID=ANY ck=140
FEATURE HI404000 metrowks 2.000 permanent uncounted A39F55AEC4D9 VENDOR_STRING="Simulator and Debugger Engine" HOSTID=ANY ck=197
FEATURE HI405240 metrowks 2.000 permanent uncounted 9FDE6FAF10F3 VENDOR_STRING="HC08 MMEVS Target" HOSTID=ANY ck=174
FEATURE HI405291 metrowks 2.000 permanent uncounted EA53C0AEE415 VENDOR_STRING="HC08 Elf/Dwarf Loader" HOSTID=ANY ck=110
FEATURE HI405293 metrowks 2.000 permanent uncounted 4AAACF68A07A VENDOR_STRING="HC08 Assembly Debug" HOSTID=ANY ck=169
FEATURE HI405294 metrowks 2.000 permanent uncounted BD0DAA8B6F78 VENDOR_STRING="4096 bytes of code, HC08 ANSI-C Debug" HOSTID=ANY ck=155
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
929 Views
Alban
Senior Contributor II
Hello Peblink,
 
May you please give some details on how CW5.0 is supposed to have crashed your computer by deleting system files......?
In my department we have roughly 20 installs of CW5.0 from CW3.1 and have no trouble whatsoever (with the installation I need to stress).
Therefore please tell us which file was supposedely affected so the CodeWarrior team can react on this "SERIOUS" accusation/problem !
 
For your license problem. I see it is a special eddition license (Free). To be sure you have a correct one, I advise you to go to codewarrior.com website and ask for a Special Edition License for CW3.1. You will be sure not to have a corrupted file.
 
The license text should be appended to the content already present in "license.dat" at the root of the installation of CodeWarrior. The text already present should not be removed, you just add the text at the end of the file.
 
Regards,
Alban.
 
(modified adding link to CW registration and licens page)

Message Edited by Alban on 2006-08-13 02:34 PM

View solution in original post

0 Kudos
Reply
1 Reply
930 Views
Alban
Senior Contributor II
Hello Peblink,
 
May you please give some details on how CW5.0 is supposed to have crashed your computer by deleting system files......?
In my department we have roughly 20 installs of CW5.0 from CW3.1 and have no trouble whatsoever (with the installation I need to stress).
Therefore please tell us which file was supposedely affected so the CodeWarrior team can react on this "SERIOUS" accusation/problem !
 
For your license problem. I see it is a special eddition license (Free). To be sure you have a correct one, I advise you to go to codewarrior.com website and ask for a Special Edition License for CW3.1. You will be sure not to have a corrupted file.
 
The license text should be appended to the content already present in "license.dat" at the root of the installation of CodeWarrior. The text already present should not be removed, you just add the text at the end of the file.
 
Regards,
Alban.
 
(modified adding link to CW registration and licens page)

Message Edited by Alban on 2006-08-13 02:34 PM

0 Kudos
Reply