S912ZVL64F0VLF lin16_cfg error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S912ZVL64F0VLF lin16_cfg error

ソリューションへジャンプ
3,414件の閲覧回数
fanziyu
Contributor IV

mcu S912ZVL64F0VLF

Problem : there is no MC9S12ZVL64 option in Global definition - MCU name  when i make npf for LIN project,so what should i do? what is more, MC9S12ZVL128.h and MC9S12ZVL64.h is different. If i choose MC9S12ZVL128,is there any problem in project development later?

thanks~

0 件の賞賛
返信
1 解決策
3,406件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

The S12ZVL64/96/128 have the same header file. So, it supports only S12ZVL128.

Therefore, you can select the S12ZVL128 instead.

 

I hope it helps.

Best regards,

Diana

 

 

Best regards,

Diana

元の投稿で解決策を見る

3 返答(返信)
3,407件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

The S12ZVL64/96/128 have the same header file. So, it supports only S12ZVL128.

Therefore, you can select the S12ZVL128 instead.

 

I hope it helps.

Best regards,

Diana

 

 

Best regards,

Diana

3,403件の閲覧回数
fanziyu
Contributor IV

Thanks for your help!

One more question:Can I just choose MC9S12ZVL128 instead of MC9S12ZVL64 in Devices page when i creat the mcu project ? otherwise,I should change some macro defintion in LIN stack files.

In practice,there be something error if i choose MC9S12ZVL64 in Devices page when i creat the mcu project and choose MC9S12ZVL128 in LIN npf file configuration.

0 件の賞賛
返信
3,379件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

Can you share the error?

I suggest using the MCU which you physically have: S12ZVL64 for your project because it has a smaller memory than S12ZVL128

 

Best regards,

Diana

0 件の賞賛
返信