S912ZVL64F0VLF lin16_cfg error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912ZVL64F0VLF lin16_cfg error

Jump to solution
3,526 Views
fanziyu
Contributor IV

mcu S912ZVL64F0VLF

Problem : there is no MC9S12ZVL64 option in Global definition - MCU name  when i make npf for LIN project,so what should i do? what is more, MC9S12ZVL128.h and MC9S12ZVL64.h is different. If i choose MC9S12ZVL128,is there any problem in project development later?

thanks~

0 Kudos
Reply
1 Solution
3,518 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

The S12ZVL64/96/128 have the same header file. So, it supports only S12ZVL128.

Therefore, you can select the S12ZVL128 instead.

 

I hope it helps.

Best regards,

Diana

 

 

Best regards,

Diana

View solution in original post

3 Replies
3,519 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

The S12ZVL64/96/128 have the same header file. So, it supports only S12ZVL128.

Therefore, you can select the S12ZVL128 instead.

 

I hope it helps.

Best regards,

Diana

 

 

Best regards,

Diana

3,515 Views
fanziyu
Contributor IV

Thanks for your help!

One more question:Can I just choose MC9S12ZVL128 instead of MC9S12ZVL64 in Devices page when i creat the mcu project ? otherwise,I should change some macro defintion in LIN stack files.

In practice,there be something error if i choose MC9S12ZVL64 in Devices page when i creat the mcu project and choose MC9S12ZVL128 in LIN npf file configuration.

0 Kudos
Reply
3,491 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

Can you share the error?

I suggest using the MCU which you physically have: S12ZVL64 for your project because it has a smaller memory than S12ZVL128

 

Best regards,

Diana

0 Kudos
Reply