Running Codewarrior v6.2/v6.3 on parallels on a Macbook OS X Lion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running Codewarrior v6.2/v6.3 on parallels on a Macbook OS X Lion

1,686 Views
karthick1987
Contributor II

Hi guys,

 

I have been having some trouble running Codewarrior V6.2 or v6.3 speical edition on Parallels on my Mac. I have attached a screenshot of the error I keep getting and I am not sure what I can do about it. I can move past this point!

 

Please advise

Thanks guys

K

 

In case you are wondering what micro I am using its a HCS08DZ128MLF (48-pin QFP)

Labels (1)
0 Kudos
Reply
2 Replies

1,553 Views
eckhard
Contributor V

Hello,

it looks like you are using Windows 7. Codewarrior 6.3 is not working with Windows 7 64 Bit Version. There are some threads here where this problem is discusssed and for some cofigurations there are solutions. I think the better way would be to install Codewarrior V10.2

Eckhard

0 Kudos
Reply

1,553 Views
karthick1987
Contributor II

Hey Eckhard,

I have Win 7 32-bit but still gives me the issue. I will try v10.2. Is it better at handling virtual machines?

Cheers

K

0 Kudos
Reply