Rename the project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rename the project

1,869 Views
frankkong
Contributor III

Hi,

  I met some problems when I rename the project(Pump for example). I use CW11.0 and the demo AN5135SW. Any suggestion?

 Rename the project.png

Tags (1)
0 Kudos
Reply
5 Replies

1,568 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Frank,

What's problme when you rename project ?

Please refer to my step have a try:

- Rename project :

pastedImage_2.png

- Change  "Build Variables" in Properteis:

pastedImage_3.png

- Then press Apply and OK buttons:

pastedImage_4.png

- Build

pastedImage_1.png

Hope it helps.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,568 Views
frankkong
Contributor III

Thanks, Alice_Yang

         I'm sorry ,it doesn't work. See my picture, it could not find include file'mc9s12zvml31.h' if I rename the project.QQ图片20180904135549.png

0 Kudos
Reply

1,568 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Fran,

After change name, please try to close the proejct, then import it again . 

BR

Alice

1,568 Views
frankkong
Contributor III

Thanks Alice_Yang,

It works!

0 Kudos
Reply

1,568 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

OK, welcome .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply