Programming in the FLASH region

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programming in the FLASH region

跳至解决方案
1,786 次查看
mmm
Contributor I
I've tried many times, but I can't store any value in the flash region, it doesn't change. (Flash because my micro, 9S08QG8 has a small RAM memory). Does the program need any espetial intruction? Or what can be the problem?
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,000 次查看
bigmac
Specialist III

Hello,

 

If your program needs additional RAM, the 9S08QG8 may not be suitable, and you will need to use a larger device.  Flash memory is read-only, and cannot be directly written like RAM.

 

It is possible to use flash memory for non-volatile storage of data, but the flash must be programmed with the required data.  This may be done from within the program code, but is much more complex than simply writing to a flash location.  There is also a finite limit to the total number of times that a flash location may be erased, and then re-programmed.

 

I suggest that you use the search engine below (for the 8-bit forum) and you should find many examples that have been previously posted. You will also need to be familar with the flash programming requirements to be found within the datsheet for the 'QG8.

 

Regards,

Mac

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,001 次查看
bigmac
Specialist III

Hello,

 

If your program needs additional RAM, the 9S08QG8 may not be suitable, and you will need to use a larger device.  Flash memory is read-only, and cannot be directly written like RAM.

 

It is possible to use flash memory for non-volatile storage of data, but the flash must be programmed with the required data.  This may be done from within the program code, but is much more complex than simply writing to a flash location.  There is also a finite limit to the total number of times that a flash location may be erased, and then re-programmed.

 

I suggest that you use the search engine below (for the 8-bit forum) and you should find many examples that have been previously posted. You will also need to be familar with the flash programming requirements to be found within the datsheet for the 'QG8.

 

Regards,

Mac

 

0 项奖励
回复