Program both P_Flash and X_Flash of MC56F8345 by Multilink Universal using one Binary File

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Program both P_Flash and X_Flash of MC56F8345 by Multilink Universal using one Binary File

2,296 次查看
HardyCao
Contributor I

Hi,

I meet a problem that program MC56F8345VFGE, I want to program P_Flash and X_Flash  where P_Flash is from 0x00000 to 0x20fff and X_Flash is from 0x01000 to 0x1ffff. and the data is stored in the same binary file where P_data is from 0x0000 to 0x20fff and X_data is from 0x42000 to 0x43fff.  how to setup the flash program? Thank a lot!

 

Hardy

0 项奖励
回复
3 回复数

2,244 次查看
HardyCao
Contributor I

Thanks a lot!

0 项奖励
回复

2,294 次查看
HardyCao
Contributor I

I use CodeWarrior 10.7, and tool is PEmicro  Multilink Universal. 

 

Hardy 

0 项奖励
回复

2,287 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach a document to describe how to use CodeWarrior for MCU tools to download S-Record file for DSC family, pls check it and have a try.

I suppose that it is okay to download code to flash for MC56F83xx family.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复