Problems with debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems with debugging

跳至解决方案
4,563 次查看
bernardinoruizg
Contributor I

Hello,

 

I am trying to debug my new project using CodeWarrior for MCU v10.6 and I am not able to debug it. I am trying to program HCS08 MCUs (MC9S08SG8 or SG32) with my USB Multilink Universal FX, but everytimeI need to program the microcontroller (on run or debug) I must power off and power on the power supply. When I try to debug, it seems to be hanged and when I click any option (pause, reset,...), I get the message: "Target request failed: HC/RS/S12Z GDI Protocol Adapter : Stop failed. Non Fatal Error."


Could anybody help me? Thank you in advance!!

标签 (1)
0 项奖励
回复
1 解答
3,896 次查看
Rick_Li
NXP Employee
NXP Employee

Hi Bernardino ruiz gonzalez,

I'm sorry for my delay replying.

if your problem still there, then, could you please upload one of your classic CW project and the ported project here for further investigating.

the problem should be caused by some problem when imported.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
3,896 次查看
Rick_Li
NXP Employee
NXP Employee

when debugging a new created project (without adding your own code), is the problem ("Target request failed: HC/RS/S12Z GDI Protocol Adapter : Stop failed. Non Fatal Error.") still there?

0 项奖励
回复
3,896 次查看
bernardinoruizg
Contributor I

No, there is no problem when I try to debug a new blank project.

The issue is that I am not creating a new code, but I am trying to port a classic CodeWarrior project into the new Eclipse IDE. All my projects were developed in the CodeWarrior v6.2 and debugged with PEMicro USB Multilink Interface. Everything works! Now I am trying to port my base software into the CodeWarrior v10.6 and debug it with USB Multilink Universal FX. I create a new project and attach the files I need. I don't know if I am doing what I am supposed to do or I need aything else.

0 项奖励
回复
3,897 次查看
Rick_Li
NXP Employee
NXP Employee

Hi Bernardino ruiz gonzalez,

I'm sorry for my delay replying.

if your problem still there, then, could you please upload one of your classic CW project and the ported project here for further investigating.

the problem should be caused by some problem when imported.

0 项奖励
回复
3,895 次查看
bernardinoruizg
Contributor I

Hi Yong Li,

I attach an example of classic project and another of eclipse project. Both attachments have 2 folders: the project and the base software (a folder with common files).

Thank you for your interest

0 项奖励
回复
3,892 次查看
Rick_Li
NXP Employee
NXP Employee

could you please check your schematic to see if RESET pin is properly connected.

the attached is a schematic for a demo board of MC9S08SG32 for your reference.

for your second problem, could you please upload an screen-shot for investigation?

0 项奖励
回复
3,892 次查看
bernardinoruizg
Contributor I

I think RESET pin is connected ok. I have attached the schematic of the board where I am testing the code.

I have also attached the error message I get when I try to debug.

Schematic.bmpCodewarriorDebugError.jpg

0 项奖励
回复
3,892 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 项奖励
回复
3,892 次查看
bernardinoruizg
Contributor I

Thank you for your advice!

0 项奖励
回复