Problem in the flash of a mc9s08pl4 with usbdm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in the flash of a mc9s08pl4 with usbdm

1,822 Views
Floppy01
Contributor I

Good morning,

I wanted to program a mc9s08pl4, after writing a simple program I compiled and clicked on debug, the debugger cannot connect with the microcontroller, the error I get 'CORBA connection error'. I use usbdm. Can anyone help me?Immagine.png

This is the code I wrote:

Floppy01_0-1625227538379.png

Thank you!

0 Kudos
Reply
3 Replies

1,815 Views
vicentegomez
NXP TechSupport
NXP TechSupport

 Is this a custom board?

 

Can you check that the DBM lines are correct, reset is correct, BKGD pin us plugged, VDD and GND 

 

Regards

Vicente G

0 Kudos
Reply

1,809 Views
Floppy01
Contributor I

Yes, I mounted the mcu on the breadboard and connected the usbdm, the following is the circuit diagram:

Floppy01_1-1625303277079.png

 

i checked the connection, they are both connected also because i tried the same circuit with a qg8 and it works.

 

0 Kudos
Reply

1,793 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check if the reset line is holding in low? did you see any signal on the BKGB line?

 

Please check all the connections, I am not sure if your USBDM is able to provide power to the board or if you also need to add power to the board.

 

Regards

 

0 Kudos
Reply