Problem going from CW10.3 to 10.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem going from CW10.3 to 10.4

跳至解决方案
3,288 次查看
pk2
Contributor III

I have a project that runs fine on a K52 that was built using CW10.3  When I build the same project in CW10.4, it only works with the debugger running.  When I try to run the code out of flash, without the debugger, the CW10.4 version does not run.  Without the debugger attached, I can't tell what is wrong.


I do not know if this is the problem but when building in CW10.4 I get 2 additional warnings:

 

Description: C:/Freescale/CW MCU v10.4/MCU/ARM_GCC_Support/ewl/EWL_C/include/ctime ignoring #pragma options align [-Wunknown-pragmas]

Resource: Myproject

Location:  line 307, external location: C:\Freescale\CW MCU v10.4\MCU\ARM_GCC_Support\ewl\EWL_C\include\ctime

Type: C/C++ Problem

 

and...

Description: C:/Freescale/CW MCU v10.4/MCU/ARM_GCC_Support/ewl/EWL_C/include/ctime ignoring #pragma options align [-Wunknown-pragmas]

Resource: Myproject

Location:  line 45, external location: C:\Freescale\CW MCU v10.4\MCU\ARM_GCC_Support\ewl\EWL_C\include\ctime

Type: C/C++ Problem

 

lines 45 and 307 are..

 

45   #pragma options align=native

.

.

.

307  #pragma options align=reset

 

Does anyone have an ideas what the problem(s) could be?

 

Gary

 

 

标签 (1)
0 项奖励
回复
1 解答
2,735 次查看
Ben
Senior Contributor I

Gary, a month ago I saw the same question which has been solved by a community member. Check if it helps

Codewarrior MQX example not running as a stand alone mode (without Debugging)

Ben

在原帖中查看解决方案

0 项奖励
回复
11 回复数
2,735 次查看
BlackNight
NXP Employee
NXP Employee

I saw a recent report where an application was not running without the debugger attached. The problem was that the 'semihosting' libraries were used. With semihosting the library (printf(), etc) tries to communicate with the debugger, otherwise it blocks. So make sure your project is *not* using semihosting. Check your project settings, under C/C++ Build > Settings > Librarian: it shall not use one of the 'hosted' options.

0 项奖励
回复
2,735 次查看
hlenahan
Contributor I

A thousand times this. I'd been practically pulling my hair out trying to figure out why my TWR-K20D72M code wouldn't start up without the debugger attached. This was the issue. And of course I couldn't find it posted until after I'd already figured it out...

0 项奖励
回复
2,735 次查看
trytohelp
NXP Employee
NXP Employee

Hi Gary,

If the problem is not solved, don't hesitate to contact us.

CW for MCU V10.5 was released last week.

You can download it from our web site:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

Last MQX V4.0.2 can be downloaded via:

      http://www.freescale.com/webapp/sps/site/overview.jsp?code=MQXSWDW

Regards

Pascal

0 项奖励
回复
2,735 次查看
pk2
Contributor III

For my application I need at least the Basic edition of CW.  Where can I find it?  Using the links above I only see the evaluation and SE editions.

0 项奖励
回复
2,735 次查看
BlackNight
NXP Employee
NXP Employee

Just one additional note: if you have a Basic Edition license for 10.3 or 10.4, you need to upgrade it to 10.5. The 10.5 release notes explain the steps.

0 项奖励
回复
2,735 次查看
BlackNight
NXP Employee
NXP Employee

The evaluation and the special edition are (binary) the same: the only difference is that the special edition does not install a license file, while the evaluation edition installs a full temporary license file for 30 days.

So you could install either of it, and then add the Basic Edition license to it. I recommend that you install the evaluation edition, then you have the full product for 30 days, and then you can use the basic edition with it.

I hope this helps?

0 项奖励
回复
2,735 次查看
pk2
Contributor III

Thanks Erich for the information.  I filled out the request to get the evaluation edition last week but no one has contacted me.  Any idea why this takes so long?

0 项奖励
回复
2,735 次查看
BlackNight
NXP Employee
NXP Employee

Hi pk,

re-reading your request: is this about the evaluation license, or about the ability to download the software?

I heard reports that the web registration process is flawed and that it believes that export control is needed.

It seems that if you enter in the forms non-standard characters (umlaut, 'foreign' characters), then you are not able to download the software :-(. so maybe this is your issue?

0 项奖励
回复
2,735 次查看
BlackNight
NXP Employee
NXP Employee

Hi pk2,

no idea :-(. Maybe your request got lost?

I'll contact you directly in order to help you out, but I suggest that you file again a request.

Sorry about that,

Erich

0 项奖励
回复
2,735 次查看
pk2
Contributor III

Pascal -

It is still nor resolved.  It is frustrating me that it does not work.  I will try CW10.5 and see if that solves my problem.

0 项奖励
回复
2,736 次查看
Ben
Senior Contributor I

Gary, a month ago I saw the same question which has been solved by a community member. Check if it helps

Codewarrior MQX example not running as a stand alone mode (without Debugging)

Ben

0 项奖励
回复