Problem With CW_MCUs_V6_0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem With CW_MCUs_V6_0

跳至解决方案
2,246 次查看
Gabo
Contributor I
Hello, I´m trying to use the evaluation version of cw 6.0 for microcontrollers, especially hc08 and hc12 and i´ve downloaded from freescale page, evaluation version, and downloaded the license.dat too, installed the program, placed the license in the installation path and wheni started the program, started a project and clicked on set (to place the path to save the project) the program just closed, it happened without setting the path too, when i click on next to start the project it closed too. I tryed to install it on other computers, downloading licences for them too and it happened all the same.
What should i do?
Thanks
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,293 次查看
CompilerGuru
NXP Employee
NXP Employee
read this thread
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Basically there is a incompatibility of MS Groove with anything running in a Windows 2000 compatibility mode.

Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,294 次查看
CompilerGuru
NXP Employee
NXP Employee
read this thread
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Basically there is a incompatibility of MS Groove with anything running in a Windows 2000 compatibility mode.

Daniel
0 项奖励
回复
1,293 次查看
Gabo
Contributor I
Thank You, it solved my problem.
Gabriel
0 项奖励
回复