Parsing Error Can't open "MK60D10.mem" file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Parsing Error Can't open "MK60D10.mem" file

跳至解决方案
5,215 次查看
GirishChoudanka
Contributor I

Hi-

 

I am using TWR K60D100M tower system with CW10.2 (Special Edition) and MQX3.8.1. I am using OSBDM for debugging purpose. The driver seems to installed correctly with current update. It get detected as COM3 on serial port. I have settings for Built Configurations as Int Flash Debug. Then I continue with Build Project (I tired Build All also) and which runs smoothly without any error. Under the Debug Configuration I have following settings:

 

Name: hello_twrk60d100m_Int_Flash_Debug_PEOSJTAG

Build Configuration: Int Flash Debug

Use Work Space settings checked

Application: intflash_d.afx

 

When I hit Debug, I get following error:

 

Failed to resume target process., There was an error parsing the memory configuration file:

Can't open "MK60D10.mem" file

("twrk60d100m.mem":20)

 

I am not sure why this error is coming or am I missing any settings? If this is not right forum then could anyone direct me to right place.

 

Regards,

标签 (1)
0 项奖励
回复
1 解答
4,587 次查看
BlackNight
NXP Employee
NXP Employee

I have attached now the full directory with all files.

在原帖中查看解决方案

0 项奖励
回复
13 回复数
4,586 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

can you check if you have that memory file (explanation of different files in the project is here: Dissection of MCU10 Projects | MCU on Eclipse)? Usually inside Project_Settings\Debugger.

The memory file is referenced from the debug/launch configuration > Main Tab > Connection > Target:memory configuration.png

0 项奖励
回复
4,587 次查看
GirishChoudanka
Contributor I

Hi Erich-

Yes, this is check in at following path

${MQX_ROOT_DIR}\lib\twrk60d100m.cw10\bsp\dbg\twrk60d100m.mem

Besides the Initialize target is at

${MQX_ROOT_DIR}\lib\twrk60d100m.cw10\bsp\dbg\init_kinetis.tcl

Does debug shift speed matters?

By default it is set to (0): MULTILINK=1.00MHz, FX=250MHz, OSJTAG=0.25MHz

0 项奖励
回复
4,587 次查看
BlackNight
NXP Employee
NXP Employee

Can you post the content of that .mem file?

Maybe the content is corrupted?

The .mem file is a normal text file.

4,587 次查看
GirishChoudanka
Contributor I

While looking in the folder dbg for twrk60d100m.mem file I came across two more files namely init_kinetis.tcl and mass_ersase_kinetis.tcl. These both file are typed aas Altium Script File as I have already Altium installed. Does this matters?

0 项奖励
回复
4,587 次查看
BlackNight
NXP Employee
NXP Employee

no, these are TCL (scripting) language files for the debugger. They are not for Altium, and have nothing to do with your problem.

0 项奖励
回复
4,587 次查看
GirishChoudanka
Contributor I

Well, surprisingly I did one thing while I was talking to PCB designer. I unchecked the .mem file and could could run debug. But then it does not run through the whole code. It just stays on dispatcher file.

With this I am seem to be lost.

0 项奖励
回复
4,587 次查看
GirishChoudanka
Contributor I

Please find below the content of the file:

// Memory Configuration File

//

// Description:

//  A memory configuration file contains commands that define the legally accessible

//  areas of memory for your specific board. Useful for example when the debugger

//  tries to display the content of a "char *" variable, that has not yet been initialized.

//  In this case the debugger may try to read from a bogus address, which could cause a

//  bus error.

//

// Board:

//  Kinetis K60DN512M10

//

// Reference:

//  -

// All reserved ranges read back 0xBABA...

reservedchar 0xBA

usederivative "MK60D10"

//         Memory Map:

//         ----------------------------------------------------------------------

range      0x00000000 0x0007FFFF 4 ReadWrite    // 512KB Code Flash

reserved   0x00080000 0x13FFFFFF

range      0x14000000 0x14000FFF 4 ReadWrite    // 4KB Programming accelleration RAM

reserved   0x14001000 0x1FFEFFFF

range      0x1FFF0000 0x1FFFFFFF 4 ReadWrite    // 64KB On chip SRAM (TCML)

range      0x20000000 0x2000FFFF 4 ReadWrite    // 64KB On chip SRAM (TCMU)

reserved   0x20010000 0x21FFFFFF

range      0x22000000 0x221FFFFF 4 ReadWrite    // Aliased to TCMU SRAM bitband

reserved   0x22200000 0x3FFFFFFF

reserved   0x60000000 0xDFFFFFFF // Flexbus for external memory

reserved   0xE0100000 0xFFFFFFFF

0 项奖励
回复
4,587 次查看
BlackNight
NXP Employee
NXP Employee

I think your problem is following line:

usederivative "MK60D10"

Could you check if you have a file MK60D10.mem in this folder (adopt the path to your installation path)

C:\Freescale\CW MCU v10.2\MCU\bin\plugins\support\Registers\ARM\mem

I think somehow your mk60d10.mem file is missing. In any case, I have attached the file I have in this folder.

0 项奖励
回复
4,587 次查看
GirishChoudanka
Contributor I

Well under this folder path I see (w.r.t. MK60)

MK60DZ10.mem

MK60N512VMD100.mem

MK60N256VMD100.mem

MK60X256VMD100.mem

but not MK60D10.

0 项奖励
回复
4,587 次查看
BlackNight
NXP Employee
NXP Employee

ok, then place my file from the above comment there and then I hope the problem will be solved for you.

0 项奖励
回复
4,587 次查看
GirishChoudanka
Contributor I

It seems you attached MK10D10.mem instead of MK60D10.mem.

0 项奖励
回复
4,588 次查看
BlackNight
NXP Employee
NXP Employee

I have attached now the full directory with all files.

0 项奖励
回复
4,587 次查看
GirishChoudanka
Contributor I

That worked!

I am able to debug the code successfully.

Regards,

Girish

0 项奖励
回复