/* This is a linker parameter file for the mc9s08lc60 */NAMES END /* CodeWarrior will pass all the needed files to the linker by command line.
But here you may add your own files too. */SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */ Z_RAM = READ_WRITE 0x0060 TO 0x00FF; // 160 byte RAM = READ_WRITE 0x0100 TO 0x085F; // 1888 byte NO_INIT_RAM_SEG = NO_INIT 0x0860 TO 0x0C5F; // 1024 byte MY_STK = NO_INIT 0x0C60 TO 0x105F; // 1024 byte NV_SAVE_SEG = READ_ONLY 0x1060 TO 0x12FF; // reserve 672 (512) byte for NV ROM1 = READ_ONLY 0x1300 TO 0x17FF; ROM = READ_ONLY 0x1870 TO 0xFEAF; FLASH_ROUTINE_SEG = READ_ONLY 0xFEB0 TO 0xFFAF; ROM2 = READ_ONLY 0xFFC0 TO 0xFFD1;/* INTVECT = READ_ONLY 0xFFD2 TO 0xFFFF; Reserved for Int. Vectors*/ENDPLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */ _DATA_ZEROPAGE, MY_ZEROPAGE INTO Z_RAM; DEFAULT_RAM INTO RAM; NO_INIT_RAM INTO NO_INIT_RAM_SEG; SSTACK INTO MY_STK; NV_SAVE_AREA INTO NV_SAVE_SEG; FLASH_ROUTINE_AREA INTO FLASH_ROUTINE_SEG; _PRESTART, STARTUP, DEFAULT_ROM, ROM_VAR, STRINGS, COPY INTO ROM; /* ROM1,ROM2 In case you want to use ROM1,ROM2 as well, be sure the option -OnB=b is passed to the compiler. */ENDSTACKSIZE 0x400VECTOR 0 _Startup /* Reset vector: this is the default entry point for an application. */
已解决! 转到解答。