PK-HCS12E128 + VMWARE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PK-HCS12E128 + VMWARE

1,167 Views
onamatic
Contributor I
Has anyone got CW / Datablaze etc. working with a usb link when Windows is hosted by VMWare under Linux?
 
My setup uses VMWare Server and it seems like it's going to work (ie: the controller halts when CW tries to communicate with it) but nothing else happens and CW / Datablaze just hang until the usb lead is disconnected.
 
I suspect it's not an easy problem to fix!
Labels (1)
Tags (1)
0 Kudos
1 Reply

348 Views
jamesarm97
Contributor II
I was hoping to use VMware also as I have a MAC. Using the P&E usb pod I was able to burn but it died right after that. I since got the AW60 demo board and the usb interface is detected but the script errors with code 45. I think during the loading of the scripts the usb disconnects then reconnects and that causes a problem.