PEMicro problems with CW 10.2 on Debian Wheezy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEMicro problems with CW 10.2 on Debian Wheezy

Jump to solution
1,762 Views
joesteeve
Contributor II

Hello all,

 

I am using Codewarrior 10.2 for Linux on Debian Wheezy. My board is a DEMOJM board: DEMO9S08MP16 Rev.B.

 

I am unable to program the board from the IDE. I setup the project to use the "PEMicro USB multilink" to connect to the board. When I do "Run>Run" it fails saying it is not able to connect to the board. It says "No device available". Hitting refresh multiple times does not help. The "PEMicro" menu is also disabled.

 

Any pointers would be of great help.

 

Thanks,

Joe

 

Message was edited by: Joe Steeve  Updated title to reflect the issue more accurately.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,014 Views
joesteeve
Contributor II

I finally solved this. You need to do the following:

Open /etc/udev/rules.d/25-pemicro.rules in an editor. Remove all its contents, and paste the following:

SUBSYSTEM!="usb", ACTION!="add", GOTO="kcontrol_rules_end"

ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="0035", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="0042", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="0058", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="005E", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="005F", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="1357", ATTRS{idProduct}=="0001", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="1357", ATTRS{idProduct}=="0503", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="1357", ATTRS{idProduct}=="0504", GROUP="plugdev", MODE="0664"

LABEL="kcontrol_rules_end"

In a root terminal:

$ ln -s /usr/lib/i386-linux-gnu/libexpat.so.1.6.0 /usr/lib/i386-linux-gnu/libexpat.so.0

View solution in original post

0 Kudos
Reply
1 Reply
1,015 Views
joesteeve
Contributor II

I finally solved this. You need to do the following:

Open /etc/udev/rules.d/25-pemicro.rules in an editor. Remove all its contents, and paste the following:

SUBSYSTEM!="usb", ACTION!="add", GOTO="kcontrol_rules_end"

ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="0035", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="0042", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="0058", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="005E", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="15a2", ATTRS{idProduct}=="005F", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="1357", ATTRS{idProduct}=="0001", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="1357", ATTRS{idProduct}=="0503", GROUP="plugdev", MODE="0664"
ATTRS{idVendor}=="1357", ATTRS{idProduct}=="0504", GROUP="plugdev", MODE="0664"

LABEL="kcontrol_rules_end"

In a root terminal:

$ ln -s /usr/lib/i386-linux-gnu/libexpat.so.1.6.0 /usr/lib/i386-linux-gnu/libexpat.so.0
0 Kudos
Reply