PE配置问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PE配置问题

1,402 次查看
春雷冉
Contributor II

我刚开始使用PE,在配置K10 I/O时,由于我需要用较多I/O,所以使用BitsIO_LDD组件,但是在设置pin的时候总是提示我Pin number differs  from requested value : 4,不知道这是为什么,

标签 (1)
0 项奖励
回复
1 回复

1,189 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please note, all pins in this component must belong to the same port and must from
contiguous set. For example in your project, the Bits1 component use Port B,
PTB16 and PTB3 not contiguous, so there is error.
You can add more BitsIO_LDD component, then add the pins PTB16-19.
Hope it helps
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------