P&E USB-ML-12 connection problem:Failed to find communication speed error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E USB-ML-12 connection problem:Failed to find communication speed error

Jump to solution
1,963 Views
raja_tata
Contributor I
Hi,
I was running fine with the codewarrior debugger(CWHC12XV4.5) on my target board having MC9S12dp256b part till today.
But suddenly, today, on the same working board, when I try to load the debugger, it gives me "Failed to find communication speed" error.Also we couldnt see USB port option  on the list of choices.
So, any ideas whether my chip has gone bad or is there anything else I can still try out.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
917 Views
Lundin
Senior Contributor IV
Most likely:
- Accidently secured processor. Try unsecuring it through the debugger option or run a separate unsecure program (available for free from PE micro if you are using their pod).

Likely:
- The BDM connector or cable is malfunctioning or turned upside down.
- Some jumper settings are messed up on the board.

Unlikely:
- The BDM pod is broken.
- The oscillator or the supply voltage circuitry is broken.

Very unlikely:
- The CPU is broken.

View solution in original post

0 Kudos
Reply
1 Reply
918 Views
Lundin
Senior Contributor IV
Most likely:
- Accidently secured processor. Try unsecuring it through the debugger option or run a separate unsecure program (available for free from PE micro if you are using their pod).

Likely:
- The BDM connector or cable is malfunctioning or turned upside down.
- Some jumper settings are messed up on the board.

Unlikely:
- The BDM pod is broken.
- The oscillator or the supply voltage circuitry is broken.

Very unlikely:
- The CPU is broken.
0 Kudos
Reply