Hi Kef,
Thank you for the info!
I am working with the M68EVB912B32 board with CodeWarrior 5.1.
I have a 12V supply to the Vpp input and connected W7 jumper to Vpp.
The PE Micro USB Multilink is connected to BDM IN (W9) on the board.
When I try to debug a simple project, I got the following error:
Communications with the target failed:
The target MCU has no clock or wrong BDM clock speed is used or derivative is secured.
In Command window, I see
Could not find appropriate io_delay_cnt.
I checked HC12MultilinkCyclonePro communication settings,
BDM Communications Speed was set to Autodetect communications speed.
Do you have any idea about this?
Also when you say NoICE, what is that? Do I need to install it?
I saw this on one webpage
Tie the MODA and MODB pins of your target to ground (Single Chip mode). If you are using these pins as port pins, you may need extra circuitry to hold the pins low during reset. In conjunction with the BDM pod, NoICE will start the chip in Special Single Chip mode. If you start in any other mode, the processor will begin executing instructions immediately, and NoICE may not be able to control it.
The MODA and MODB pins are not used on my board, should I worry about it?
Thanks!
Yuping