P&E Full Chip Simulator Cycle Counter in CW v10.x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E Full Chip Simulator Cycle Counter in CW v10.x

Jump to solution
1,847 Views
carloscuev
Contributor V

Hello, I would like to know if there's any cycle counter in full chip simulation in the new CW v10.x Like the great one that CW v6.x had:

 

 

Getting the difference of CPU Cycles between a function entrance and fuction exit was a great way to test for function efficiency doing subtle changes in how a function operates :smileyvery-happy:

 

I'm really getting used to CW 10.2 but I need this feature. Thanks !

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,406 Views
carloscuev
Contributor V

I was desperate searching for the solution of my NEW ISSUE :smileysad: and found the answer to this one, it's in the PEmicro menu:

 

 

Haven't tested it though, I'm really desperate with the new issue. Hope it works !

View solution in original post

0 Kudos
Reply
4 Replies
1,405 Views
carloscuev
Contributor V

Well I've tested it and found a bug.

 

I've explained it here: 

http://www.youtube.com/watch?v=lMSU_T_9_7U

 

But with the workaround I explain also there it's usable.

0 Kudos
Reply
1,407 Views
carloscuev
Contributor V

I was desperate searching for the solution of my NEW ISSUE :smileysad: and found the answer to this one, it's in the PEmicro menu:

 

 

Haven't tested it though, I'm really desperate with the new issue. Hope it works !

0 Kudos
Reply
1,406 Views
BlackNight
NXP Employee
NXP Employee

oh right! I have missed that one.

 

Thanks!

BK

0 Kudos
Reply
1,406 Views
BlackNight
NXP Employee
NXP Employee

Hello,

this does not exist in Eclipse (yet). I have asked P&E about it, but to my knowledge it is not there yet.

 

BK

0 Kudos
Reply