On chip flash programming in MC68HC908QB8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

On chip flash programming in MC68HC908QB8

跳至解决方案
2,873 次查看
kuji83
Contributor I
Hi,
In MC68HC908QB8, How can we access the falsh area and do page erase, Programming and Check or Compare programing. Any conversant c code available to all functions.
 
We would like to erase the falsh area and update with datas and do comparision with them and store these values.
 
Awaiting for reply.
 
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,432 次查看
J2MEJediMaster
Specialist I
Go the FAQ system and search for "Flash programming". A number of FAQs on the subject should show up. You'll have to sift through these for your MCU. Some of them reference Application notes, which document how to use a feature, such as programming Flash, and even provide source code.

---Tom

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,432 次查看
kuji83
Contributor I
Thank you very much for your help.I have wriiten the flash routine.
0 项奖励
回复
1,432 次查看
bigmac
Specialist III
Hello,
 
The application notes AN2635 and AN2874 cover use of the ROM-resident routines, present within the QB8, and other HC908 devices.
 
Regards,
Mac
 
1,432 次查看
CrasyCat
Specialist III
Hello
 
Did you check application notes on Freescale web site?
 
There might be something in there.
 
CrasyCat
0 项奖励
回复
1,433 次查看
J2MEJediMaster
Specialist I
Go the FAQ system and search for "Flash programming". A number of FAQs on the subject should show up. You'll have to sift through these for your MCU. Some of them reference Application notes, which document how to use a feature, such as programming Flash, and even provide source code.

---Tom
0 项奖励
回复