已解决! 转到解答。
You can use sprintf function that is part of the std C lib.
Or I made the following code to build a String with a converted number added to it using the following code. The first function combines some of the standard C string functions along with the Integer to Ascii conversion. I use integers in C with assumed decimal points. This is limited as to the number of digits. The code can be modified to use long intergers if needed.
Example - I have a timer value that as an integer it is 9999. But as the user sees it after conversion it is 9.999
I define the Digits and Decimal positions
#define DELAY_TIMER_DIGITS 5
#define DELAY_TIMER_DECIMAL 1
int TimerValue = 9999;
char MyString[30];
To build a string to display to user with format of x.xxx for TimerValue
ItoaMsg(&MyString[0], "Delay Timer = ", TimerValue, DELAY_TIMER_DIGITS, DELAY_TIMER_DECIMAL);
I then print MyString on the display which would be "Delay Timer = 9.999"
void ItoaMsg(char *Buffer, char *Msg, INT16 Number, char Digits, char Decimal) {
/* Local variables */
char Array[11];
/* Convert Number to string */
Itoa(Number, Digits, Decimal, &Array[0]);
/* Copy Msg to Buffer */
(void) strcpy(Buffer, Msg);
/* Add Number string to Buffer */
(void) strcat(Buffer, &Array[0]);
}
/* Integer to ASCII */
void Itoa(INT16 Number, char Digits, char Decimal, char *String)
{
/* Get starting position in string array */
char *PositionSave, *Position = String + Digits;
/* Negative flag */
char NegativeFlag = FALSE;
/* Charactor buffer */
char Chr;
/* Working UINT16 */
UINT16 uInteger;
/* Loop index */
INT16 Index;
/* Number of digits converted */
INT16 DigitCount = 0;
/* Make sure we are converting more than one digit */
if(!Digits)
return;
/* Are we working with a negative number? */
if (Number < 0) {
/* It is a negative number */
NegativeFlag = TRUE;
/* Remove the sign bit from the integer */
uInteger = ((UINT16)(-(1 + Number))) + 1;
} else {
/* Not a negative number */
uInteger = Number;
}
/* NULL terminate the string */
*Position = 0;
/* Do the conversion */
do {
/* Decrement the digits counter */
Digits--;
/* Get the ASCII charactor */
*--Position = '0' + (uInteger % 10);
/* Divide by 10 */
uInteger /= 10;
/* Have we reached the end of the number? */
if(!uInteger)
break;
/* Increment the digit counter */
DigitCount++;
} while (Digits);
/* Do we need to add a decimal point? */
if(Decimal && Digits) {
/* Remove another digit position */
Digits--;
/* Do we have enough space for a leading 0? */
if(Digits && (DigitCount < Decimal)){
for(Index = Decimal - DigitCount; Index > 0; Index--) {
*--Position = '0';
DigitCount++;
Digits--;
if(!Digits)
break;
}
}
/* Decrement and save the pointer */
Position--;
PositionSave = Position;
/* Move the charactors */
for(Index = DigitCount - Decimal; Index >= 0; Index--) {
Chr = Position[1];
Position[0] = Chr;
Position++;
}
/* Insert the decimal point */
*Position = '.';
/* Restore the pointer */
Position = PositionSave;
}
/* Do we need to add the negative sign? */
if (NegativeFlag && Digits) {
/* Add the negative charator */
*--Position = '-';
/* Reduce the digit count */
Digits--;
}
/* Do we need to pad any charactor positions? */
for(Index = Digits; Index != 0; Index--)
*--Position = ' ';
}
You can use sprintf function that is part of the std C lib.
Or I made the following code to build a String with a converted number added to it using the following code. The first function combines some of the standard C string functions along with the Integer to Ascii conversion. I use integers in C with assumed decimal points. This is limited as to the number of digits. The code can be modified to use long intergers if needed.
Example - I have a timer value that as an integer it is 9999. But as the user sees it after conversion it is 9.999
I define the Digits and Decimal positions
#define DELAY_TIMER_DIGITS 5
#define DELAY_TIMER_DECIMAL 1
int TimerValue = 9999;
char MyString[30];
To build a string to display to user with format of x.xxx for TimerValue
ItoaMsg(&MyString[0], "Delay Timer = ", TimerValue, DELAY_TIMER_DIGITS, DELAY_TIMER_DECIMAL);
I then print MyString on the display which would be "Delay Timer = 9.999"
void ItoaMsg(char *Buffer, char *Msg, INT16 Number, char Digits, char Decimal) {
/* Local variables */
char Array[11];
/* Convert Number to string */
Itoa(Number, Digits, Decimal, &Array[0]);
/* Copy Msg to Buffer */
(void) strcpy(Buffer, Msg);
/* Add Number string to Buffer */
(void) strcat(Buffer, &Array[0]);
}
/* Integer to ASCII */
void Itoa(INT16 Number, char Digits, char Decimal, char *String)
{
/* Get starting position in string array */
char *PositionSave, *Position = String + Digits;
/* Negative flag */
char NegativeFlag = FALSE;
/* Charactor buffer */
char Chr;
/* Working UINT16 */
UINT16 uInteger;
/* Loop index */
INT16 Index;
/* Number of digits converted */
INT16 DigitCount = 0;
/* Make sure we are converting more than one digit */
if(!Digits)
return;
/* Are we working with a negative number? */
if (Number < 0) {
/* It is a negative number */
NegativeFlag = TRUE;
/* Remove the sign bit from the integer */
uInteger = ((UINT16)(-(1 + Number))) + 1;
} else {
/* Not a negative number */
uInteger = Number;
}
/* NULL terminate the string */
*Position = 0;
/* Do the conversion */
do {
/* Decrement the digits counter */
Digits--;
/* Get the ASCII charactor */
*--Position = '0' + (uInteger % 10);
/* Divide by 10 */
uInteger /= 10;
/* Have we reached the end of the number? */
if(!uInteger)
break;
/* Increment the digit counter */
DigitCount++;
} while (Digits);
/* Do we need to add a decimal point? */
if(Decimal && Digits) {
/* Remove another digit position */
Digits--;
/* Do we have enough space for a leading 0? */
if(Digits && (DigitCount < Decimal)){
for(Index = Decimal - DigitCount; Index > 0; Index--) {
*--Position = '0';
DigitCount++;
Digits--;
if(!Digits)
break;
}
}
/* Decrement and save the pointer */
Position--;
PositionSave = Position;
/* Move the charactors */
for(Index = DigitCount - Decimal; Index >= 0; Index--) {
Chr = Position[1];
Position[0] = Chr;
Position++;
}
/* Insert the decimal point */
*Position = '.';
/* Restore the pointer */
Position = PositionSave;
}
/* Do we need to add the negative sign? */
if (NegativeFlag && Digits) {
/* Add the negative charator */
*--Position = '-';
/* Reduce the digit count */
Digits--;
}
/* Do we need to pad any charactor positions? */
for(Index = Digits; Index != 0; Index--)
*--Position = ' ';
}